Event History

The Event History section provides a detailed record of all events detected by the system over a selected time period.

Event history

  1. Click Event history to view events that occurred within a specific time frame.

  2. Show/Hide filter: Enable the following options.
    • Dimension type: Allows you to select dimension types and apply filters based on the configured dimensions of the metric.

    • Date range: Allows you to select the desired date range for viewing events.

Event timeline

The Event timeline provides a chronological visualization of key events, including their types and corresponding dates.

The legend visually distinguishes event types using color codes:

  • Critical events - Red

  • Warning events - Yellow

  • Mixed events - Black

  • Normal events - Green

Display tiles

  • Total events: It displays the total number of events recorded during the selected time frame.

  • Critical events: It displays the number of high-severity events logged by the system in a given period.

  • Warning events: It displays the number of moderate-severity events detected during the selected period.

Event table

Fields

Descriptions

Event type

The system categorizes events into the following types:

  • Critical: Indicates a serious issue that requires immediate attention.

  • Warning: Indicates a potential problem or an early indication of an issue.

  • Normal: Indicates standard or expected system behavior.

Dimensions

Leverage up to two dimensions to segment and analyze data.

Value It represents the numeric result of the calculated metric associated with the event.
Event start time

Indicates the exact date and time when the event was triggered or first detected by the system.

Event end time

Indicates the exact date and time when the event concluded or was last recorded by the system.

Duration

Indicates the total length of time an event remained active—from the Event Start Time to the Event End Time.